我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
What connector is used to make the BMXFTW301 cable?

Issue:
Connector used to make the BMXFTW301 cable


Product Line:
M340, BMXFTW301


Resolution:
The BMXFTW301 is simply a BMXFTB2020 terminal block with a color coded flying lead cable attached to it.

Cable pinout