我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Does the ION/SPM/PME OPC client have the ability to do OPC writes to a third party OPC server?

Issue:
Power Monitoring Expert has a built in OPC DA client used to connect to third party OPC DA servers. Customer would like to know if this client has the ability to write to the OPC DA tags in addition to being able to read it.

Product Line:
ION Enterprise 6.0.x
Struxureware Power Monitoring Expert 7.0.x
Power Monitoring Expert 7.2.x
Power Monitoring Expert 8.x

Environment:
OPC Client

Resolution:
No. The built-in OPC client  in ION/SPM/PME does not have the ability to write to 3rd party OPC servers.