我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
What is the range of value that Arithmetic module supports in VIP ?

Issue
User would like to know the range of value that Arithmetic Module supports in VIP (Designer)?

Product Line
ION Enterprise, StruxureWate Power Monitoring Expert 7.0.1, PME 7.2.x, PME 8.x

Cause
User would like to know the maximum and minimum range supported with Arithmetic Module within VIP.

Resolution
For Arithmetic module in VIP, the data type of the output register is 64 bit floating point. Therefore, it allows a range from -10 ^ 308 to +10 ^ 308.