我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
In G system, which weight can the slotted plates withstand?

The weight allowed on slotted mounting plate03170, 03171, 03172 and 03173 is 30kg maximum.
Pay attention in System G about the risk of falling for floor standing enclosure


Legacy KB System (APS) Data: RESL182415 V4.0, Originally authored by SeOs on 03/01/2007, Last Edited by GwPo on 06/25/2010
Related ranges: Prisma Plus