When viewing a custom diagram in WebReach the text 'WebReachDefaultDiagramNode' is displayed under all/some objects, but this label is not shown when the diagram is viewed in Vista.
Resolution
- Open the diagram in Vista
- Select all the objects that are displaying this problem.
- Right-click on one of the objects.
- In the Caption tab, change the Caption selection from Use Default to None.
- Save your changes and reload the diagram in WebReach
發佈於: 施耐德電機Taiwan