我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
What is the Modem initialization string for the ION7650 and ION7550?

Issue
Modem initialization string for the ION7550/7650

Product Line
ION7550
ION7650

Environment
Communication Protocols

Resolution
The modem initialization string for the ION7650 and the ION7550 is 'AT&F' (without the quotes).