我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Do the RJ45 Modbus RS232 ports of the TSXETG100 and the 174CEV30020 have the same pinout?

No the RJ45 Modbus RS232 ports of the TSXETG100 and the 174CEV30020 do nothave the same pinout.
The pin assignments of the ports are as follows: