我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Tutorial: Data Quality Tool

Goals and Symptoms

General Overview of Data Quality


  • Definition of Data Quality

    • Data quality refers to the quality of data. Data are of high quality "if they are fit for their intended uses in operations, decision making and planning" (J.M. Juran). Alternatively, the data are deemed of high quality if they correctly represent the real-world construct to which they refer. These two views can often be in disagreement, even about the same set of data used for the same purpose.