我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
How long can the overvoltage condition last on the metering inputs of the Series 4000 Circuit Monitor (CM4000)?

Issue
Limits of the CM4000 overvoltage conditions

Product Line
CM4000

Environment
Product Specifications

Cause
Over voltage conditions that the CM4000 can sustain before failure

Resolution
From Table B-1 of Appendix B in the CM4000 reference manual, the meter allows a 50% metering over-range of voltage. The meter can handle this overvoltage condition indefintely.

施耐德電機Taiwan

附件
CM4000_Reference_Manual.pdf [3.41 MB]