我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
What is the amount of SF6 gas in 24 kV SF Circuit Breaker range.
In 24 KV SF Circuit Breaker range, the weight of the SF6 gas per pole for different Circuit Breakers is as follows:
  1. SF1 Type 1 – 49 grams
  2. SF1 Type 2 – 112 grams
  3. SF2 – 240 grams