我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
How is the ATV312 default display changed to show a different monitored parameter?
Issue:
Display a different monitored parameter on an ATV312

Product Line:
ATV312  ATV31

Environment:
All

Cause:
Preference is to normally display a parameter such as motor current or motor torque, not the factory default of output frequency.

Resolution:
Go to SUP menu and display the parameter to be used as a default display ( e.g. LCr or Otr ).  Press ENT once to show the current value of that parameter.  Then press and hold ENT for about 2 seconds and the display will flash, indicating the process is complete.