我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Where are the basic wiring diagrams for an S-FLEX ?
Issue:
Basic wiring diagrams for an S-FLEX

Product Line:
S-FLEX 212

Environment:
All

Cause:
Needed for wiring and troubleshooting.

Resolution:
The standard wiring diagrams for units with and without the bypass feature can be found in the  S-Flex™ 212 Adjustable Speed Enclosed Drive Instruction Bulletin, document# 30072-451-83.
See attachments. Note that there have been design changes for bypass versions over the years.  The current bypass design is series E.

施耐德電機Taiwan

附件
SFlex212 with Bypass series E.pdf [188.08 KB]
SFlex212 with Bypass series D.pdf [153.55 KB]
SFlex212 without Bypass.pdf [106.06 KB]
SFlex212 with Bypass.pdf [159.72 KB]