我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
What is the part number for the M221 24 vdc power connector?
Issue:
Is there a part number to order the power connectors for the M221?

Product Line:
M221

Cause:
Customer misplaced the connectors and requires new ones.

Resolution:
The part number for the 24 vdc power connectors for 24 vdc is TMAT2PSET and this is a set of 5 removable screw type connectors.