我們的品牌

Impact-Company-Logo-English Black-01-177x54

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
What will cause enclose units not to run the motor in AFC or in Bypass?
Issue:
Enclosed units not to running the motor in AFC or in Bypass.

Product Line:
SFLEX, EFLEX, MFLEX, CPD, MCC, Field Drive, Econoflex, 58M

Environment :
All Enclosed products with Bypass

Cause:
The motor will not run in AFC or in Bypass

Resolution :
1).  Check supply fuse primary side of transformer.
2).  Check fuse on the secondary side of the transformer
3).  Verify the overload is not tripped, (trip and then reset)
4).  Verify the AFC/OFF/Bypass switch is getting voltage
5).  With factory drawing in hand check the HOA and the AFC/OFF/Bypass circuit.

施耐德電機Taiwan

探索更多
產品:
探索更多
產品: