我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
While Importing xml file in the BMXNOR0200 firmware version V1.6 there is error saying import not successful ?
Issue: When user imports the XML, the error "Import not Successful appears"

Product Line: BMXNOR0200 V1.6

Environment: Unity Pro V12

Resolution:

The XML file contains the module and protocol configuration parameters. One can easily export these parameters into a XML file.
This file can later be restored into the module by importing it from the module webpage.
However if the module communication  channel parameters are not defined, then you get an error import not successful while importing the xml file.


Communication channel preferences

So its very important to define the communication channel parameter before exporting the configuration into the xml file.