我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Where can I find information on the ATS48 analog output?

Article available in these languages: 西班牙文

Issue:
Information on the ATS48 analog output?

Product Line:
ATS48

Environment:
All models and serial numbers

Cause:
None

Resolution:
The analog output can be assigned to reflect one of the following:
1. motor current
2. motor torque
3. motor thermal state
4. Power factor
5. active power
The analog output can be scaled between 50 and 500%.  For a more detailed explanation of the scaling and parameters please see the attached.

施耐德電機Taiwan

附件
ATS48_AO Analog output assignment calculation.pdf [413.36 KB]