我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Can a CM2000 handle 2 wire RS-485 communication?
Issue
2-wire RS-485 serial communication available on the CM2000 series meters

Product Line
CM2000 series

Environment
Communications, RS-485

Resolution
A CM2000 can only do 4 Wire RS-485 communications. A 2 to 4 wire converter (such as a CNV-100) is required in order to add a CM2000 to a 2 wire daisychain.