我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
How to use Unity Pro or EcoStruxure Control Expert simulator on Windows 8.1, 10 and Windows Server 2008, 2012, 2016
On Windows 8.1, 10 or Windows Server 2008, 2012 or 2016 for some applications the Unity Pro or EcoStruxure Control Expert simulator is starting with exception.
To avoid this wrong behavior, launch the attached file, and reboot the PC.

Other possibility is to modify or to create manually, as below, some keys inside the Windows registry:

For 32 bits Windows versions
HKEY_LOCAL_MACHINE\SOFTWARE\Microsoft\Windows NT\CurrentVersion\Image File Execution Options\sim.exe, Name "DisableExceptionChainValidation", REG_DWORD, value 1.

For 64 bits Windows versions
HKEY_LOCAL_MACHINE\SOFTWARE\WOW6432Node\Microsoft\Windows NT\CurrentVersion\Image File Execution Options\sim.exe, Name “DisableExceptionChainValidation", REG_DWORD, value 1.

施耐德電機Taiwan

附件
DisableException.zip [413 Bytes]