我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
What are the voltage, temperature and altitude tolerances for the Altivar 32/320 drive?
Issue:
Customer wants to know the temperature and altitude limitations for the ATV32/ATV320 drive.

Product line:
ATV32, Altivar 32, ATV320, Altivar 320

Environment:
All

Cause:
n/a

Resolution:
The voltage range for the M2 drives (200-240V) is 200V, minus 15% to 240V, plus 10%.
The voltage range for the N4 drives (380-480V) is 380V, minus 15% to 480V, plus 15%.

The temperature rating for all models is +14F to +122F (-10C to +50C), without derating (as long as the switching frequency is 4 kHz or less).

Optional derating is available from +122F to +140F (50C to 60C).  Consult the Installation manual for de-rating curves based on the temperature and switching frequency.

The maximum altitude the Altivar 32 can be installed without de-rating is up to 3300 feet (1000 meters).  De-rate the drive nominal current by each additional 330 feet (100m) up to a maximum ceiling of 10,000 feet (3000m).