我们今天能为您提供什么帮助?

PlantStruxure PES [V4.0]: Why am I not able to scroll to see the full contents of the Instance Editor?

Goals and Symptoms

To scroll to see the full contents of the Instance Editor


Facts and Changes

PES version V4.0


Causes and Fixes

Increase the height or width of the Instance Editor window by dragging its bottom or right-hand edges.
Before:
image1
After:

image2