我們的品牌

Impact-Company-Logo-English Black-01-177x54

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
I cannot connect to the M580 CPU with Unity Loader
By default, the M580 CPU's ftp service is disabled (preferred option for cyber security ).
Unity Loader will not connect if it cannot establish connection to ftp.
To enable ftp on your CPU (with SV<=3.20), load an application into the CPU, that has FTP enabled. You can enable in Control-Expert in the Security Tab of the  ethernet ports configuration of the M580 CPU :
capture