我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
What are the dimensions and weight of the ATS48C11Y?
Issue:
Needs the dimensions and weight of the ATS48C11Y

Product Line:
ATS48

Environment:
ATS48D62Y, ATS48D75Y, ATS48D88Y, ATS48C11Y

Cause:
N/A

Resolution:
Width - 7.48 "
Height - 11.42"
Depth - 9.25"
Weight - 18.3 lbs