我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
ComX connection issues with GPRS in Facility Insights
Issue
The ComX is not connected to the remote platform

Product Line
Com'x

Resolution
  1. Confirm there is no proxy presently configured. If a proxy is configured, consult your network administrator.
  2. Validate GPRS Signal is at minimum 3/4 on the ComX Web page. If signal is below this level, increase signal via an external antenna.