我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
What is included in the ATVPOT25K potentiometer kit?
Issue:
ATVPOT25K potentiometer kit

Product Line:
Altivar accessory

Environment:
All models

Cause:
None

Resolution:
The ATVPOT25K pot kit is for use with any Altivar VFD.  It includes:
Potentiometer 22mm operator, ZB5AD922
Potentiometer, 80442-273-02, 2.5k Ohm
Legend holder, ZBZ32
Legend and Misc hardware not offered separately.

The pot operator has graduation marks only, no designations. The legend is marked "Manual-Speed Pot".

施耐德電機Taiwan

附件
ATVPOT25K.png [154.55 KB]