我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
What causes error "Unknown header in the file:" when downloading Unity firmware?
Issue:
Dowloading Unity copro or executive firmware displays error.

Resolution:
If flashing the CoPro firmware, make sure you are using FTP protocol.
If NOE, use FTP protocol.
Is the .bin / .ldx file correct for the PLC type?