我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
What data types are supported by the Real Time Tables in PME and SPM?

Issue:
There are measurements available on a device such as a device's serial number and volts mode. However these measurements are not available for selection in the real time tables

Product Line:

Power Monitoring Expert 9.0

Power Monitoring Expert 2020

Power Monitoring Expert 2021

Power Monitoring Expert 2022

Power Monitoring Expert 2023

Power Monitoring Expert 2024



Environment:
Web Applications Real Time Tables

Cause:
Real Time Tables support only certain data types. The measurements that do not appear in the list of available measurements are of a type that is not supported.

Resolution:
Real Time Tables only supports the following data types: numeric, date, boolean.

String type such as device type, serial number and volts mode cannot be displayed.

Recommendation:

If you are using an older version of PME, consider upgrading to the latest version for improved protocol support and security. For assistance with integration or upgrades, contact Schneider Electric Technical Support at: pmo-psup@se.com

Support information