我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
When under voltage error is triggered, how to automatically reset LXM28.
P2-66.
This bit specifies the type of Fault
Reset after a detected undervoltage error
has been removed.
0: No automatic Fault Reset
1: Automatic Fault Reset