我们今天能为您提供什么帮助?

What is the F10 fault on a TR Inverter/Charger?

Environment:

12V or 24V DC battery systems

Cause:

F10 indicates a high battery voltage condition:

Above 15.5 V on a 12 V system
Above 31 V on a 24 V system

This typically occurs when the batteries are wired incorrectly, or an external charging source is pushing the voltage too high.

Resolution

Verify the batteries are connected in the correct configuration for the system (12V or 24V).
Check for external chargers, alternators, or solar controllers causing over‑voltage.

施耐德電機Taiwan

探索更多
產品:
探索更多
產品: