我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Will SoMove display the VW3A3408 resolver option cards serial number, part number or firmware version?
Issue:
Is SoMove showing option card serial number, part number or firmware version?

Product Line:
Altivar 71 only with the VW3A3408 resolver option card

Environment:
All

Cause:
Wants to know if SoMove will display the serial number, part number and firmware number.

Resolution:
SoMove will only display the reference part number of the card only see example below.

nh