我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
ION 7300 Tran-Eth DB26 cable wiring pinout
Issue
Older ION 7300 series TRAN–ETH models used a high density DB26 connector as the interface to the Remote Modular Display instead of DB-25. The cable was a special DB26 to DB25 male to female and it’s not available for purchase any longer.

Ion 7300 Trans-Eth DB26

Product line
ION 7300 Tran-Eth with a DB-26 port

Resolution
The customer needs to create their own DB26-to-DB25 cable based on the wiring pinout below :
DB26-DB25 wiring pinout