我們的品牌

Impact-Company-Logo-English Black-01-177x54

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Is it possible to input 400V 50 Hz to a drive and get 460V 60 hz out?
Issue:
Is it possible to input 400V 50 Hz to a drive and get 460V 60 hz out?

Product Line:
All drives.

Environment:
All

Cause:
Available Input 400V 50 Hz to the drive and need  460V 60 hz out

Resolution:
It is not possible to get more voltage out of a drive than what is coming in.