我們的品牌

Impact-Company-Logo-English Black-01-177x54

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
How much current is available on the ATS48 +24V power supply?
Issue:
ATS48 +24Vdc power supply specifications.

Product Line:
ATS48

Environment:
All models and serial numbers

Cause:
None

Resolution:
The 24Vdc power supply can provide up to 200mA.