我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
What is the maximum current rating of an ATS22 relay?
Issue:
Maximum current rating of an ATS22 relay.

Product Line:
Altistart 22, ATS22

Environment:
All

Cause:
N/A

Resolution:
Max switching capability:
5A - 250VAC or 30VDC on resistive load (p.f.=1)
2A - 250VAC or 30VDC on inductive load (p.f=0.4)