我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Can the phase loss protection on the ATS48 soft starter be turned off?
Issue:
Can I turn off the phase loss protection on the ATS48?

Product Line:
ATS48

Environment:
All model number, all serial numbers

Cause:
N/A

Resolution:
No, the PHF cannot be turned off. Parameter PHL (Phase Loss Threshold) can be adjusted between 5% or 10%.