我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
What is the operating system on the Harmony HMIGTO series?
Issue:
The user manual of the Hamrony HMIGTO does not indicate what operating system is pre-installed from the factory.

Product Line:
Harmony HMIGTO series (formerly known as Magelis)

Resolution:
The Harmony HMIGTO series of HMI's have the Operating System VxWorks V6.7 embedded inside.