我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Cannot change the FTP password for the BMXNOR0200 using Web Designer.

Issue
Cannot change the FTP password for the BMXNOR0200 using Web Designer.

Product Line
BMXNOR0200

Environment
Windows 10

Resolution
The selection for FTP password on the target security window is greyed out and not selectable.
tryu


Due to cyber security reasons, the ability to change the FTP password for BMXNOR RTU Factorycast module using
Web Designer is not allowed.   Changing of the FTP password for the  BMXNOR0200 RTU Factorycast module must
be performed from the 'Setup' web pages.