我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Why doesn't the dynamic text in my Message Display update as the variable changes?
Issue:
Text in Message display is not updating according to the value of the variable embedded.

Product Line:
Vijeo Designer (all versions)

Resolution:
When using Dynamic Text, the value shown is a single snapshot of the current value of the variable being displayed at the moment it is displayed. The value of the dynamic text is not updated until the next state change of the message display.