我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Does Schneider Electric offers a Magelis Box without a touchscreen panel running on VxWorks?
Issue:
Does Schneider Electric offers a Magelis Box without a touchscreen panel running on VxWorks?

Product Line:
Magelis Box PC,

Resolution:
Schneider Electric does not offer any Magelis Box (without a monitor) that is running VxWorks.  The closest one to that specifications is the HMIG3U.

Schneider Electric offers a Magelis Box without a touchscreen panel running on VxWorks? | 施耐德電機Taiwan