我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Sepam 80 - is it possible to order spare plastic connectors for the MES120 module?
Yes.  In the 2014 edition of the Sepam 80 "Operation" user manual, the reference given refers to the MES114 instead of the MES120.

The reference 59676 does indeed refer to the "Kit 2640" which includes 2 sets of the 3 plastic connectors that are required for each MES120 module.


AEDL3