我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Is there a controller inside card option for ATV630 process drive?
Issue:
Controller optional inside card for ATV630 process drive.

Product Line:
Altivar ATV630

Cause:
Wants to know if they can get an IMC card for the ATV630 drives?

Resolution:
No there is not an option for a IMC card on the ATV630 drive.