我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
What can cause a CF12 fault [Download transfer fault] on an ATV212 drive?
Issue:
CF12 fault [Download transfer fault] on an ATV212 drive.

Environment:
All models and serial numbers

Cause:
The download transfer fault can be caused by parameter F807 not being set to 0.

Resolution:
Parameter F807 selects the communication channel.  The two choices are 0 [RJ45] and 1 [Open style].  The default setting is 1.  If SoMove or the IPAD app is being used to configure the drive parameter F807, then it must be set to 0.