我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
How to get the detail data between DTM in UP and X80 HART module
The communication bwteen DTM and HART module is HART over ethernet, we can capture the trace by wireshark at the service port of CRA if the HART is configured at the RIO Drop, the CRA service port should be configured mirroring the eth backplane.
Refer to the attachment picture, we can get the HART frame in the CIP data field, we can understand it following the HART command protocol.

施耐德電機Taiwan

附件
Microsoft PowerPoint - [Expert Support webinar - X80 HART Rev3- Jan. 28th.pptx]_2.jpg [90.27 KB]