我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Can I connect aluminium or copper, flexible or rigid cables to the single and double terminals of the NSX 400 to 630 range.?
In the NSX 400 to 630 range:

Single terminals, part numbers LV432479 or LV432480, can take: aluminium or copper rigid cables with cross-section 35 to 300 mm² and flexible cables with cross-section 240 mm² maximum.

Double terminals, part numbers LV432481 or LV432482, can take: aluminium or copper rigid cables with cross-section 35 to 240 mm² and flexible cables with cross-section 185 mm² maximum.

施耐德電機Taiwan

附件
ghd16312aa.pdf [788.25 KB]