我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Do we need to install Vijeo Designer Runtime to download to a Magelis HMI?
Issue:
It is unclear what the Vijeo Designer Runtime for Windows package is intended for.

Product Range:
Vijeo Designer 5.1 or higher

Resolution:
The Vijeo Designer Runtime for Windows executable does not need to be installed to download to a Magelis HMI. This installer is only intended to be used on iPCs or PCs that will be used as an HMI. You do not need to install this package on the Vijeo Designer development PC.