我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Can you use the VW3A1101 keypad on the ATV12 drives?
Issue:
Wants to use the VW3A1101 keypad on the ATV12 drives.

Product Line:
Altivar ATV12

Environment:
All

Cause:
Customer wanted to know if he can use the VW3A1101 keypad on the ATV12 drive.

Resolution:
The VW3A1101 keypad will not work on the ATV12 drive.  You will need to use the VW3A1006 or VW3A1007 keypad display.