我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
ATV630 Process drive with Ethernet IP option card how do you set it up to use assemblies 103 and 104?
Issue:
ATV630  Process drive with Ethernet IP option card setting it up to use assemblies 103 and 104.

Product Line:
Altivar ATV630 ATV650 ATV660 etc

Environment:
All

Cause:
They needs to set up the ATV630 drive with the optional Ethernet IP card to use assemblies 103 and 104.

Resolution:
The ATV630 Ethernet IP card VW3A3720 does not support assemblies 103 and 104.  You will have to configure your PLC's Ethernet Scanner module for assemblies 100 and 101.