我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
How to delete a DTM in a Unity pro application when not installed - M340 platform

Issue

Error message displayed when trying to delete a DTM
Potential issue due to the DTM version Compatibility"
"Warning: Potential issue due to the DTM version incompatibility.... DTM.
An error occurs during the check of DTM compatibility. DTM version in application is Vx).
DTM on the PC: not installed or installed without version information

Product Line

M340

Resolution

As of today, when a DTM is not installed,  it is impossible to create the dynamic menu of the Dtm and then delete it.

We suggest to

  • Install the required DTM
  • Update the DTM catalog
  • Open the application and the TOOL>DTM browser
  • Delete the desired DTM from the DTM browser tree.