我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Why my M241/251 controller stops in exception when an SD card is inserted?
One reason can be that the inserted SD card has no label.

To set the SD card label:
- open Windows file explorer
- select the SD card
- press F2 to rename it (for example : "mySDcard")