我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Video: How to duplicate a trend in the PME 8.x Web Applications
Issue
A user would like to duplicate an existing trend in the Power Monitoring Expert Web Applications.

Product Line
Power Monitoring Expert (PME) 8.x

Environment
PME Web Applications Trends

Resolution
  1. Open the Power Monitoring Expert Web Applications.
  2. Click on the Trends tab.
  3. Expand the menu on the right side of the screen if not already expanded.
  4. Click on the trend you wish to make a copy of on the right hand menu.
  5. Click the duplicate option at the top of the right hand menu pane. (This is the second option from the left)
  6. Make desired changes to the trend and click ok.
The new trend will be displayed below the original.

Please also reference the following video for more details.