我们今天能为您提供什么帮助?

[Modicon M580 HSBY] How to avoid broadcast storm when using mixed RIO and DIO architecture with BMENOC03x1

It is necessary to disable the Ethernet backplane port of each BMENOC03•1 communication module.
please find the following picture to find where to disable the ethernet backplane port.

施耐德電機Taiwan

附件
Capture.PNG.png [36.54 KB]